I use a tmux1219 to switch a voltage signal between 2.5VRef and 5Vref by a gpio pin from a stm32. I find that the U13 tmux1219 often does not work normally. The circuit diagram see attachment.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use a tmux1219 to switch a voltage signal between 2.5VRef and 5Vref by a gpio pin from a stm32. I find that the U13 tmux1219 often does not work normally. The circuit diagram see attachment.
Hi
Adding to what Clemen's asked, Could you also check what does the signal look like if you remove the mux (U13) and short the signal path
Can you provide details on "often does not work" - What is the behavior you see when it does not work?
Can you take scope shots at inputs and output of the mux?
Are you using 5.5V supply for the mux?
Regards
Saminah
In some times, I can not switch S2 to D when SEL pin is high, it is always switch on S1 whether SEL pin is high or low, and the D pin is always 2.5V.
In other some times, the D pin is always 2.58V whether SEL pin is high or low.
SW.VEX.SEL is a GPIO from stm32 MCU, I measured the signal, it can be set to 0V or 3.3V according my intention.
When I weld a new tmux1219 chip, it is work normal at once, it can switch to S1 or S2, and the D pin is 2.5V or 5V accordingly. But, after a period of time(for example one day or 5 days) it can not work normal and can not be recovered again.
Hi,
Can you share the scope shots at input and output pin of U13 (both when working and non-working).
When you say "it can not work normal and can not be recovered again" - what signal do you see at "D"?
Can you make sure you are following the design recommendations for the TMUX1219 as shown below:
Regards
Saminah
Hi,
It is ok to not have the decoupling and pullup/pull down resistors on select pins buy you need to make the device is performing under recommended operating conditions
Can you confirm if your supply to TMUX1219 is 5.4 V - the schematic shows VCC + A5V4
When the U13 is not working as required, can you probe VDD, GND and select pins of U13 as I mentioned earlier and share the scope shots - it could be the device is losing ground and you don't see it functioning after some time.
Regards
Saminah