Hi team,
Do we need to add pull-up resistors for terminal A or B? Thanks!
Best regards,
Sam Ting
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Do we need to add pull-up resistors for terminal A or B? Thanks!
Best regards,
Sam Ting
Hi Sam,,
CB3T device is a down translator
The way the part works is it is an N-channel which will output Vcc-1v. There is an internal pullup type circuit that uses the input signal to pull it up to the Vcc level. That is why the input must be 1V higher than Vcc.
Here is another e2e thread with similar question:
Regards
Saminah