Hello,
I'm using the sn74cbtlv3251.
In all unconnected pins (i.e. not selected in S0,S1,S2) I measure a voltage of about 0.6~0.7 volts. In the selected pin i measure 3.3V
Even if oe is high, I see this voltage.
My setup is:
VCC = 3.3V
A = 3.3V.
OE = 0V or 3.3V with 10kohm pullup.
I thought the device put all unconnected pins to high Z.
What is wrong?
Thanks,
Ofer.