Hello,
I would like to use the SN74CBT16209AD as a two 9-bit bus multiplexer, only using the functions A1=B1 or A1=B2. I will supply the chip with 5VDC and I do not want to perform any level translation. I would like to clarify the following points:
-What are the VOH and VOL levels for inputs that can be TTL 3.3 or 5V (VCC=5VDC)?
- Unused A2 pins, can be left floating?
- Is available any reference design?
Thank you so much.
Best Regards