Other Parts Discussed in Thread: SN74HC4066
Hi,
I am replacing the SN74HC4066 with the TMUX1511 switch but since I am using only 1 of the 4 channels, should I ground the source of the 3 unused channels? The SEL control inputs have weak 6Mohm pull downs to prevent the switch from turning on, but if these inputs are still actually CMOS, should they be grounded if unused (i.e. S2, S3, S4)?
Thanks