Hi,
I have a question about ΔICC in data sheet P5.
Does ΔICC mean that the drive capacity of each CH is 2.5mA max?
Or does ΔICC mean that the maximum sink current of the control terminals (1OE, 2OE, S0, S1) is 2.5mA?
Best regards,
Hiroshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question about ΔICC in data sheet P5.
ΔICC does not apply to the data channels, and the control inputs always have high impedance.
The control inputs work best with 5 V logic signals. ΔICC describes how much more current flows (into VCC and out of GND) when you apply a lower voltage to one of them. See section 4.6.28 of Understanding and Interpreting Standard-Logic Data Sheets.