Other Parts Discussed in Thread: TMUX1237, TMUX1219,
Hello Support team,
Could you provide Comparison table of TMUX1219, TMUX1237, and TMUX1247? What is difference of each device?
Thanks,
Koji Ikeda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Koji,
See below for a quick spec comparison table (all single values are typical values at VDD = 5V)
All three of the parts are similar, but they each have there strong points.
The TMUX1219 is better when you don't need more than 30mA of current to pass through the switch, and you are looking for a lower leakage option this is the best part.
The TMUX1237 can handle a higher current as well as pass the highest frequency signals as well with a typical bandwidth of 400MHz
The TMUX1247 is similar to the 1237, but with a slightly lower bandwidth.
If you have any other questions please don't hesitate to reach out!
Best,
Parker Dodson