This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A21366: Can IN1/2 = 3.3V when use 1.8V at Vcc

Part Number: TS5A21366

Hi Team,

Can IN1/2 = 3.3V when use 1.8V at Vcc?

Based on spec, the maximum input voltage is Vcc. It seems like this violate spec.

Shaq