Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MUX506: Current Channel

Part Number: MUX506

Hello Team,

My Customer would like to know if the input current of each channel is 30mA or the total current through all of the channels is 30mA?

Thanks in advance,

Regards,

_Renan

  • Hey Renan,

    MUX506 is a 16:1 multiplexer with 4 address lines to choose the channel that will be used. This rating is for the total current through a single channel, seeing as how only one channel can be selected at a time. There shouldn't be any significant current through the other channels. 
    Keep in mind that this is the absolute max and the recommended range is from -25mA to 25mA


    Thanks,
    Rami