Other Parts Discussed in Thread: SN74CBTLV3253, , TMUX1309, TS3A5017-Q1, TMUX1574
Hi,
my customer is using SN74CBTLV3257 and SN74CBTLV3253, but now they need extend the operating temperature to 105C.
What's the best pin to pin upgrade part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
my customer is using SN74CBTLV3257 and SN74CBTLV3253, but now they need extend the operating temperature to 105C.
What's the best pin to pin upgrade part?
Howard,
The SN74CBTLV3257-EP has a temperature range of -55 to 125 and is p2p with the non-EP version.
What package are they using for the 3253? The only p2p is the TS3A5017-Q1 but it's the VQFN package only. This would be a good choice for the 3253 if powered-off protection is important. A good replacement for a non-P2P device would be the TMUX1309 if powered-off protection isn't an important feature for the customer.
Let me know if these work or if there's any other support you may need.
Thanks,
Rami
Hi Howard,
TMUX1574 is a newer device and a replacement for the SN74CBTLV3257 device. The device is available in industry standard TSSOP, uQFN and small SOT-23 leaded package. This device has wider supply voltage. higher bandwidth and supports -40C to 125C temperature.
Additional features include 1.8V logic compatibility, Fail-safe logic (control pins can be powered before supply), and Powered-off protection.
Thank you,
Sandesh