This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3125: SPICE Model for use with TINA

Part Number: SN74CBTLV3125
Other Parts Discussed in Thread: TMUX1511,

Need an unprotected model of this part that will work with TINA- model on web is encrypted and won't work.

  • Hello,

    Could you explain more about the issue you are experiencing? The HSPICE models are in fact encrypted but this should not prevent you from being able to set up test benches and simulate.

    If possible, you may want to try another simulation software, such as PSpice for TI or Keysight ADS. Could you try one of these and let me know if you are still experiencing the same issue?

    I would also like to add that TMUX1511 is a great, newer replacement for SN74CBTLV3125 with improved specifications and features. A PSpice model is available for TMUX1511.

    Thanks,
    Kate