Other Parts Discussed in Thread: TS5A3357
Hello
We are testing the TS5A3359 to be able to switch between an SD card and an EMMC memory but unfortunately, we are experiencing some performance issues.
The device works ok on its own, we tested it with a signal generator and all inputs and outputs are working correctly, the problem is when we want to read from the SD card, as the host PCB doesn't seem to be able to detect the SD card connected.
The weird thing about this is that if we connect an oscilloscope to probe from the N0/N1/N2 side, where the SD card is, the SD card is detected. Needless to say that we only need to connect the oscilloscope probe to 1 signal, it can be any, for the SD card communication to work. Any ideas on why this could be happening?
It will be worth mentioning that the required pull-up resistors for the SDA lines are connected on the COM side of the multiplexor only. Is it required to have pull up resistors in both signal sides of the multiplexor?
See schematics below.