The Pspice model of TS3A27518ERTWR is not correct and unusable. It cannot be recognized by the pspice simulator.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Pspice model of TS3A27518ERTWR is not correct and unusable. It cannot be recognized by the pspice simulator.
Hi Yong,
TI provides an Hspice model for this device, therefore it would not be compatible with a pspice simulator. You would either need to convert the existing Hspice model to a Pspice model or use an Hspice compatible simulator.
Thanks!
Bryan
Hi Bryan,
I guess you misunderstand my question. It's not tool issue, it just the ts3a27518_process.lib file issue.
You can open it with windows note and you can see the messy code which cannot be used.
Please help to check it.
Thank you.
Hi Yong,
The Hspice model that is available for this device is an encrypted model and hence you will not be able to read as simple text. You should still be able to simulate it using an Hspice simulator (not Pspice simulator).
Also, if you are setup for S-parameters simulation, here is another thread that links those files.
Thank you,
Regards,
Sandesh
Thanks Sandesh. It seems that this part has no Pspice module for board-level simulation. Should use Hspice for IC-level netlist simulation.
Hi Yong,
We have taken a note on this Pspice request for future support and have added it our development queue.
Thank you!
Bryan