Other Parts Discussed in Thread: TMUX1574
Hi, Can the device use in below application?
- I2C
- SPI
- CAN
- UART
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Can the device use in below application?
Hi Jim,
It depends on what voltage and bandwidth these communication protocols are being used at. The SN74CBTLV3257 has a maximum bandwidth of 200MHz and supplies that can pass signals up to 3.3V. Will that be sufficient for the requested application?
If not, we have a newer part that should meet all of your requirements which is the TMUX1574 that can support up to 5.5V and 2GHz bandwidth.
Let me know if you have any additional information on your exact application and I can help pick the correct part.
Thanks!
Bryan