Hi
I want to make it clear the specification of Analog signal voltage.
I could not get the meaning of the following note.
[Absolute Maximum Ratings]
Analog signal voltage(4) –0.5(min) VCC + 0.5 V(max)
(4) This value is limited to 5.5V (maximum).
According to the note (4), Analog signal voltage seems to be limited by 5.5V as maximum.
Is this always applicable?
For example:
When VCC=0V, could the analog signal voltage accept 5.5V?
BestRegards