Other Parts Discussed in Thread: TS3A24159
Hi
Can we use TS3A24157 or TS3A24159 for UART switching like this manner with 115200 communication baud rate
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Louis for the guidance
In my design MASTER A is TMS570LS0714PGE and MASTER B is PIC16LF7515 while SLAVE device is XBEE S2C PRO, all are operating on 3V3 power supply
So i think there is no any signals which exceed the recommended specs...
What do you want to say about it...?
your guidance is very helpful for me .....
Hello,
If that is your operating voltage, then correct, this should work.
Your baud rate of 115200 will be 115.2kHz, which is significantly slower than the max operating speed of this switch at 3V3.
I have attached a snippet of the TS3A24157 below speced at 3V Vcc and highlighted the BW of the device:
Thank you for sharing your application in such detail with us, it really helps us provide you the best support that we can.
Louie
If I have answered your questions, please hit the Verify Answer button.