Part Number: TS5A22362
Other Parts Discussed in Thread: TS5A22366
e2e,
I have another question related to the TS5A22362 I was hoping you could help with.
The input logic high (min) is 1.4V for both 2.7 and 3.3V operation of the TS5A22362, but I wonder if a 1.8V control voltage would lead to excessive current draw as described in the below appnote.
http://www.ti.com/lit/an/scda011/scda011.pdf
We have the TS5A22366 that supports 1.8V logic operation but input leakage at 1.8V Vin is nearly 1 uA with V+ = 3.6V. Do you have data for what the leakage is at 1.8V Vin (and ideally 3.0V supply) for the 22362?
Thank you,
Adam