This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: Application in HDMI. HDMI 2.0 impedance test fail.

Part Number: TS3DV642

Hi,

    I using TS3DV642 in HDMI application, In HDMI 2,0 impedance test fail.

    When I tested the HDMI impedance of TS3DV642, The same channel, there is no problem in testing HDMI1.4.

    When testing HDMI2.0, the impedance exceeds the standard, the same card. Without using the HDMI channel of TS3DV642, the impedance is normal.

    For the HDMI channel that has been added to the TS3DV642, How to make it pass the impedance test of HDMI1.4 and HDMI2.0 simultaneously?

    Normal data and increase TS3DV642 corresponding channel exceeded data such as annex.

    Normal impedance in HDMI 1.4 test:(it limit is 100ohm +-15%)

   

    Abnormal impedance in HDMI 2.0 test:(it limit is 100ohm +-10%)

   

thanks.