This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 234
Part Number: TS5A23167
Hello,
I have a customer using P/N TS5A23167YZPR (DSBGA package), BGA package shown pin is A1, B1, C1, D1, A2, B2, C2, D2.
But Datasheet shown Pin 1, 2, 3, 4, 5, 6, 7, 8. The footprint and symbol shows A1, B1, …
Could you please tell us how to match the pin from 1, 2, … 8 to A1, B1, C1… D2?
Assume A1=Pin1, B1=Pin2, C1=Pin3, D1=Pin4, A2=Pin5 or Pin8?....?
Regards-Mike
Michael,
Pin 1 is A1 and
Pin 2 is B1
Pin 3 is C1
Pin 4 is D1
Pin 5 is D2
Pin 6 is C2
Pin 7 is B2
pin 8 is A2. Thank you, Adam