Other Parts Discussed in Thread: TMUX136, TMUX1072
Hi,
As per the datasheet the ON capacitance for TS3A5223 part is shown as 115pF.
I think 115pF ON capacitance of the switch is definitely higher side and may causing ringing/possible oscillation.
So does that mean during ON period the impedance going to be as follows based on the frequency of the input signals :
Constant |
Pi |
ON Cap |
10Mhz |
2PifC |
Impedance |
2 |
3.141 |
1.15E-10 |
1.00E+07 |
7.22E-03 |
1.38E+02 |
Constant |
Pi |
ON Cap |
20Mhz |
2PifC |
Impedance |
2 |
3.141 |
1.15E-10 |
2.00E+07 |
1.44E-02 |
6.92E+01 |
In our design we do have the differential signals coming from catheter connected to ADL5565ACPZ and the output of this IC is connected to the switch as above.
We want to make sure if it is not going to load the IC due to ON capacitance !