This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 339
Part Number: TS3A24157
Hi,
I'm noticing that the minimum signal voltage under "absolute maximum ratings" is listed as -0.5 V. Is this supposed to represent the DC level, or the minimum signal swing? I have an application where the input signal (max frequency of about 6 MHz) has a 0V DC level, but swings between +0.5V and -0.5V. Would this be okay, or would this degrade the life of the part? Due to SI concerns in the low-frequency, I'd like to avoid using a blocking cap and bias network if at all possible.
Thanks,
Charles