Other Parts Discussed in Thread: TS3A5018
Hi Sir,
For SN74LV4053A application, is Y port used for input and COM port for output ?
Does it has data rate limitation ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
For SN74LV4053A application, is Y port used for input and COM port for output ?
Does it has data rate limitation ?
Anne,
The SN74LV4053 device is bi-directional and either the Y or COM pins may be used as inputs or outputs.
Yes all FET switches have bandwidth limitations. The -3dB bandwidth for the SN74LVXXXX devices is 50 MHz.
Additional information about these questions can be seen in the application report selecting the right TI signal switch.
What are you connecting to this switch? What is the data rate and signal voltage of the application?
Thank you,
Adam