Hi team,
my customer need SPDT 2:1 solution, but 1 input is 1.8V and another is 3.3V.
do we have single chip solution to do?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
my customer need SPDT 2:1 solution, but 1 input is 1.8V and another is 3.3V.
do we have single chip solution to do?
Bonnie,
These signals switches are bidirectional passive FET switches and will pass any voltage from one side of the switch to the other with out issue. If you set Vcc to the highest voltage you need to pass you can place 3.3V on one input and 1.8V on another input. The TS3A5223 will handle this without issue.
Thank you,
Adam
Bonnie,
The voltage level on the COM pin depends on what is driven to the NC or NO pins and which signal path is selected. The TS3A5223 doesn't source or sink any current by itself. You can think of the TS3A5223 ideally as a wire.
Thank you,
Adam
Hi Team,
We need the component to support NC pin 3.3v/1.8v input and COM pin output 3.3v, so the level shift function is for the NC pin not SEL pin.
Could you help to provide other chip to meet the request?
Hi Adam,
so back to my question, so we don't have signal switch conbine with level shifter function, right?