Part Number: TS5A3159-Q1
Other Parts Discussed in Thread: TS3A27518E-Q1
Does anyone have an idea of what the propagation time of this switch is under these conditions:
1) the 'IN' pin (pin 6) is static at say logic high (This is the switch control pin)
2) A pulse is sent in on pin 4 'COM and measured on pin 1 'NO'
3) The supply is +5V.
What is the propagation time between the rising edge on the pulse seen at pin 4 and measured at pin 1.
There is a 'Turn on time' parameter stated in the datasheet but this is switching pin 6 when pin 4 (COM) is static.