This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TS5A4624: I2S signal switching

Expert 2975 points

Replies: 3

Views: 717

Part Number: TS5A4624

Hi team

My Customer requested MUX/Switch for I2S communication like the below.

So, I will suggest TS3A44195 and TS5A4624.

Is it ok that TS3A44195 and TS5A4624 apply I2S communication for the follow?

Please check and reply.

  • Charles,

    I2C signals are typically 3.3V and 400kHz to 1MHz and I2S is 3.3 V 12MHz to 25MHz. Can you confirm the voltage and datarates for your I2C and I2S bus?

    This means you will need to choose a switch that can support 3.3 V signal and have a bandwidth of at least 3 times your highest frequency signal(75 MHz if you are using 25MHz I2S as your fastest signal.)

    Since you will need 2 channels for I2C and 4 channels for I2S, I would recommend using 3x TMUX1209 devices which are 2-channel 4:1 devices.

    Thank you,
    Adam
  • In reply to Adam Torma:

    Hi Adam

    I changed block for the below.

    Check please.

  • In reply to Charles Jeon:

    Charles,

    The main difference between the TCA9546A and the TMUX1209 is how you give the switch the signal to change state.  The TCA9546A requires a full I2C command from the microcontroller to change the switch state where the TMUX1209 simply uses a GPIO high or low signal to change state.  Another main difference is the TCA9546A can communicate to all 4 ISPs simultaneously where the TMUX devices can only communicate one at a time.

    Why did you choose to use the TMUX1104?  

    The lowest IC count solution is using 3x TMUX1209 devices. 

    Thank you,

    Adam 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.