Hi,
This device is announced to enable 3.3v to 2.5v shifting.
According to its datasheet, the level shifting is done as described in the following picture (taken from the datasheet):
According to what said above, if I want to get VOH=2.5v I need to connect VCC=2.5V since "The output high voltage (VOH) level will be equal to approximately the Vcc voltage level".
On the other hand, it is said that to get VOH=VCC, the VIH level be greater than or equal to Vcc+1v and less than or equal to 5.5v which means :VIH>=Vcc+1v=3.5v.
So if VIH shall b bigger than 3.5v (VIH>=3.5v) in order to get VOH=2.5v than how can that Level shifter make it for VIH=3.3v or little bit less (DC drop till the device) ??