Hi
My Application :
Iam planing to use "TMUX6111" as pass through Switch for the RS232 Signals ? Is is okay
Can use Single Power supply +12 Volt DC?
Thanks
K.Baskaran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My Application :
Iam planing to use "TMUX6111" as pass through Switch for the RS232 Signals ? Is is okay
Can use Single Power supply +12 Volt DC?
Thanks
K.Baskaran
K.Baskaran,
You may power the TMUX6111 device with a single supply by setting Vss to 0V and Vdd any voltage between 10 and 33 V as stated in the recommended operating conditions. However the voltages on the signal path S and D may not exceed the Vss and Vdd range. Make sure your RS232 do not go negative when operating the TMUX6111 in single supply operation.
What is your RS232 voltage range?
Thank you,
Adam