Part Number: TMUX136
Hi dear supporting team,
customer want to use TMUX136 to switch BTW CML & LVPECL level the detail as below:
1. input to port1.
2. when the input is 10Gsps CML signal, output from port1 without any matching.
3. when the input is 1Gsps LVpecl signal, output from port2 with 150 ohm Rt at the output to GND at each side.
if customer could accept the signal loss at 5GHz for CML. is it ok to use it in this way? (i.e. add Rt after the mux for the LVEPCL signal, will the Ron/Con affect LVPECL?)
TKS A LOT!