Other Parts Discussed in Thread: TS12A12511
Hello,
I'd like to use the TS3A44159 to switch between RS422/RS485 RX and TX (4 wire full duplex communication) for easier cabling. Switching between directions at the transciver is no option for me because of active EMI filtering. Since there may be EMI surges on the transmission line (EN61000-4-5 8/20µs) I'm using the ESD1014 for camping which has a maximum clamping voltage of 11V. That's the maximum input protection I can offer.
So may question:
Has the TS3A44159 any surge rating at the analogue input?
Or can you guarantee that the clamping is sufficient?
Thank's in advance and kind regards,
Guenther