Other Parts Discussed in Thread: TS5A22362, TS5A22364, TS5A22366
Hi Experts,
I have customer using TS5A23157 for years. Now we have one new user case for MIC differential signal switch.
Please see the design sch. as below.
Some questions that need your help as below.
Thanks.
-
For TS5A23157, is it good for audio signal application ?
-
As below spec, the absolute negative voltage tolerance is -0.5V, while the recommended is 0V. But for the customer application, the MIC input signal has swing amplitude that below 0V, and the peak negative value could be down to -0.47V, see as below or attachment waveform.
Could you help check if any risk to damage the pin ?
-
And for the -0.5V limit in spec, is it because of ESD clamp protection? What’s the time level that the PIN could tolerate -0.5V ? like 10ns, 100ns ?
-
For the application with peak-peak amplitude larger than 1V, that is, negative cycle could be more than 0.5V, should we add one DC bias like 1V or above, to avoid the negative voltage happen at IC pin ?
Thanks.