Hi ,
I want a little confused about the usage of MUX509. When the input source is float like TC or ultrasonic transducers, can MUX509 work with just postive 12V power?
I see the input range is VSS to VDD. But for these signal source, they don't have dc voltage relative to the system ground. Maybe there is a bias voltage after the chip(On the D pin), But s pin is still float.