Part Number: SN74CB3T1G125
Other Parts Discussed in Thread: LSF0101
The model provided does not have the capability to set for output. It can be only set for input.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74CB3T1G125
Other Parts Discussed in Thread: LSF0101
The model provided does not have the capability to set for output. It can be only set for input.
Lok Wei,
Input/Output Buffer Information Specification (IBIS) models only apply to buffers. The SN74CB3T1G125 only has a buffer on the control logic pin whoes output controls the internal circuitry of the IC to turn on and off the signal path. The signal path can though of as a passive FET switch and not a buffer which is why there isn't an output option. The signal path simply passes the signal from one side of the switch to the other.
Why are you using the SN74CB3T1G125 instead of a level shifter product like the LSF0101?
Thank you,
Adam
So, the IBIS model does not have the accessibility on pins 2 & 4 (A & B)? Several clarifications as:
a.) Inputs 0 to 5 V oscillation signal with 150 MHz to pin A.
b.) Outputs observation at pin B.
I'm not be able to choose LSF0101 as the bandwidth is not high enough as mentioned 150 MHz.
Thanks.