This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A4624: TS5A4624DCKR Propagation Delay

Part Number: TS5A4624
Other Parts Discussed in Thread: SN74AUC2G53, , SN74LVC2G53

I can’t find propagation delay parameter VNC or VNO-> VCOM  delay in datasheet. Could you help provide it?

  • Hi Paul,

    We don't have the propagation delay spec in the datasheet. However if you can provide details on the voltage signal swing, the type of signals you are using and the protocol you are running?

    The propagation delay is the calculated RC time constant of the typical on-state resistance of the switch and the specified load capacitance, when driven by an ideal voltage source (zero output impedance). If you know your loading conditions (RLC), those can be used to determine the propagation delay.

    How did you come across TS5A4624 switch - We do have some 2:1, 1 channel switches with propagation delay specs (SN74LVC2G53, SN74AUC2G53) that you can consider depending on your application requirements.

    Thanks

    Saminah