This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4053B: Can CD4053B accept Hot Swap?

Part Number: CD4053B
Other Parts Discussed in Thread: TMUX1133

Hi team,

My customer is using 2 CD4053B to switch 1 SPI port to 2 connectors. The block diagram is as below picutre. The SPI datarate is less than 10Mbps. The connector 1 and connector 2 will be connected to some external module. But the external module will do Hot Swap with the connector 1 or 2. So my question is:

1. Can CD4053B data port endure Hot Swap with external module?

2. The Rdson of CD4053B is relatively high. Is it OK to switch the 10Mbps SPI signal?

3. CD4053B is an old device, do we have any new device to use here?

Best regards,

Wayne

  • In general, all analog switches support hot swapping (they do not care about the voltage at their I/O pins). If the switch is currently closed, the device behind the switch will see anything that happens at the connector.

    In any case, all external connections require ESD protection.

    The Ron, combined with the trace/cable/connector capacitance, will form a low-pass RC filter. For 10 Mbps, it's probably fine. If in doubt, look at an oscilloscope trace.

    To find better devices, use the search function.

  • Hi Wayne,

    Voltages at the analog I/O pins of all switches may change, but should remain within recommended operating conditions for best performance.

    Please see Clemens' response about ESD protection, Ron, and the search function.

    TMUX1133 is a newer device with low Ron and higher bandwidth. I have included the device comparison below:

    Regards,

    Kate

  • Hello,

    Just checking in that your question was answered. I am marking the case resolved, but please don't hesitate to post a reply if you have any more questions!

    Regards,

    Kate