This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't get footprints!!! UltraLibrarian-created script throws an error in Altium 19!!!

Other Parts Discussed in Thread: TMUX136

I need a PCB footprint for TMUX136. I found that the data sheet does not contain this information but that TI supplies this in a .bxl format which is to be translated by UltraLibrarian into library files for my CAD package, which is Altium. That's a great idea and would be very convenient if it worked. However, it doesn't. I run UltraLibrarian to create the Altium script files, I follow all of the readme directions and upon trying to execute the script Altium gives me the error: "Undeclared identifier: GetFontID". Then it sets a breakpoint in the script and the only way to get out of the situation is to stop the script. I can't step past, I can't edit the script, I am stuck.

How do I get a footprint for this device? I attempted a dxf export as a workaround, but the dxf that UltraLibrarian created was... sub-standard. I have to say that this would have been a better-executed idea if you'd left footprint drawings in the data sheets and supplemented (instead of replacing) that information with this automatic-generation method. Then at least I'd have a backup source of information.

Can anyone help me out here?