Other Parts Discussed in Thread: TS5MP645, TMUX1574
Hi Team,
Do TI have 2:1 switch solution, to switch between LPC and eSPI?
8 bit Bidirectional, Max bus speed 66.67MHz
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tiffany,
Thanks for posting to E2E.
We do not have a switch of this same configuration (8-channel 2:1 switch). We do have TS5MP645 which may be suited for your application as it is a 10-channel 2:1 switch.
Additionally, you may want to consider TMUX1574. TMUX1574 is a great 2:1 switch for SPI applications, however it only has 4 channels. TMUX1574 has several features such as 1.8V logic compatibility and powered-off protection.
Let me know what you think!
Regards,
Kate