Part Number: SN74CBTLV1G125
Other Parts Discussed in Thread: TMUX1101, TS5A3167,
Hi Team, we would like to ask the information of the ESD Rating and Class.
Thank you very much
Regards,
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74CBTLV1G125
Other Parts Discussed in Thread: TMUX1101, TS5A3167,
Hi Team, we would like to ask the information of the ESD Rating and Class.
Thank you very much
Regards,
Mark
Hi Mark,
What is the application and end equipment for this device?
I would like to recommend switching to a newer device, if possible. TMUX1101 is a great option with wider supply signal range, lower Ron and leakage current, 1.8V compatible control inputs, and fail-safe logic.
If you need powered-off protection for your application, take a look at TS5A3167 which also has wider supply signal range, lower Ron and leakage current, with added powered-off protection.
Both TMUX1101 and TS5A3167 have +/-2000V ESD HBM ratings.
Regards,
Kate
Hi Kate,
Thank you for responding. However, the customer wants to know the ESD rating of SN74CBTLV1G125 since they already started the design.
I hope you can help us.
Thanks.
- Mark
Hi Mark,
This part is an older device and does not have a specified ESD rating. However, engineering data indicates performance for the SOT-23 (DBV) package up to:
HBM: 1500V
CDM: 500V
Best regards,
Kate