We are using a TS5A3166 in some of our products and was wondering if you would explain the notes 4 and 5 in the data sheet, in the abs max table.
Are these notes referring to the ESD diode inside and if input voltage exceeds the Vcc +0.5V then it starts to conduct through the diode using a small amount of current until it reaches the diodes clamping voltage? Also what is the power rating of the diode?