This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 70
Part Number: TMUX1208
Hi Team,
If I have unused "S" input pins, what should i do with them? Leave them floating or ground?
Thank you,
Jared
Hi Jared,
Switch channel inputs can either be left floating or terminated to GND (which can help reduce signal reflections). However, switch logic inputs, such as Select pins, OE pins, and other logic inputs, should never be left floating. They should be, by default, tied to either VCC or GND.
This is also mentioned in the FAQ below:
Thanks
Saminah