Hi Team,
I want to use TMUX1574 in my research, but i don't understand, when i use VDD=3.3V input S1A=1.8 V the output D1=?? V.
Is input voltage = output voltage?
Thank you and best regards,
Chou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I want to use TMUX1574 in my research, but i don't understand, when i use VDD=3.3V input S1A=1.8 V the output D1=?? V.
Is input voltage = output voltage?
Thank you and best regards,
Chou
Hi Wen,
As Clemens mentioned, the TMUX1574 has very low RON of 2-Ohm - besides that the output will be impacted by your loading conditions.
The TMUX1574 offers very low and flat RON because of the switch structure (See more details in the video, What are common switch architectures?) and supports bidirectional analog and digital signals on the source (SxA, SxB) and drain (Dx) pins and can pass signals above supply up to VDD.
Thanks
Saminah