Hi,
Can this mux be used for FSI signals?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vino,
The FSI is a serial communication peripheral capable of high-speed communications, up to 200 Mbps.
What is the datarate requirement for your application?
For digital applications we recommended the switch bandwidth be 1.5 times the datarate per lane.Bandwidth requirement for FSI @ 200Mbps would be ~300MHz
The TS3A27518E supports bandwidth of 240MHz.. Are you going to use all 6 channels of this device?
You can also look at the TMUX1574 is a 2:1, 4 channel switch that supports a higher bandwidth of 2Ghz.
Regards
Saminah