This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS5A3166: possible operation mode

Prodigy 120 points

Replies: 1

Views: 39

Part Number: TS5A3166

Good day,

One of my customer plans to use TS5A3166 and there is a question about possible operation mode. Can this device held impulse with following parameters or it will be damaged: amplitude from -0.6V to -9V (negative voltage relative to ground), duration is from 200 μs to 1ms, current is less than 100mA. There is a schematics below. Impulse is applied to pin (1).

Thank you,

Daria

  • Hi Daria,

    The TS5A3166 does not support negative voltage on the signal path - -0.6V to -9V will be operating outside the absolute maximum conditions (even for a short duration) that can damage the device.

    In similar configuration, you can look at the TS12A4516/7 that supports negative signals.

    Regards

    Saminah

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.