This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TS5A23167: TS5A23167YZPR

Prodigy 160 points

Replies: 2

Views: 72

Part Number: TS5A23167

Hi, I don't see a Tpd (propagation delay) information in a data sheet.

Please, assist to get.

Youry

  • Hi Youry,

    The TS5A23167 is a passive FET switch and have almost no propagation delay due to the silicon die.  The significant portion of the delay is due to the bond wire and packaging.  Typically the packages these switches are in have single digit ns to ~100s ps propagation delay. 

    It should not be the critical path for most applications. 

    Please also refer to the E2E post on more information regarding propagation delay of typical FET switches. 

    Regards

    Saminah

  • In reply to Saminah C:

    Thank you

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.