This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 70
Part Number: SN74CB3Q3257
Hi,
Can you advise whether SN74CB3Q3257 is suitable for i2c interface application?
Or
Is there a better solution in 2:1, 4 channel that supports I2C.
Thanks
Saminah
Saminah,
I think I answered part of this question in another thread, I’ll link it here.
The BW (f3db = 500Mhz), I/O current specs (+-64mA max), on-capacitance (10.5pF typical), on-resistance (4 ohm typical), should be sufficient to support I2C communication. The SN74CB3Q3257 2:1, 4-channel, SPDT, is specifically designed for data intensive applications, and has a max switching frequency foe = 20 Mhz.
I could recommend the 2:1, SPDT, 4-channel, TMUX1574, which is p2p (pin to pin) compatible to the SN74CBTLV3257 which is p2p compatible to SN74CB3Q3257.
The TMUX1574 is an upgrade from the SN74CB3Q3257. TMUX1574 supports more features like I/O signal voltage beyond supply, a higher BW (2 GHz), lower on-capacitance (7.5pF), lower on-resistance (2 ohm), and more.
Hope this helps!
Regards,
Tyler