Part Number: TMUX1072
Other Parts Discussed in Thread: TMUX136
Team,
See use case below:
-What is the best MUX choice for I2C interface?
-Do you advise to use TMUX1072, TS5A623157 or other?
At the system level it is important that the communication does not get disturbed by IEC61000-4-4 Burst events.
The setup is as below:
On a PCB an I2C master communicates to an I2C slave over an analog MUX (like TMUX1072, TS5A623157). IEC61000-4-4 Burst events could occur on the Master side I2C (before the MUX) and the communication might get disturbed:
I2C master <------------> MUX <------> I2C Slave
|
ESD burst
-What TI MUX is better suited for such scenario?
-Do we have some design advises/guidelines (schematics, PCB layout) that can help to mitigate such issues?
-Would ESD protection (such as TPD2E2U06 ) be the best to mitigate those type of problems?
-Any TI reference design that specifically tackle IEC61000-4-4 Burst events creating interface communication issues with Analog MUXes?
Thanks in advance,
A.