This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4067: Internal protection diodes inside CD74HC4067 or CD74HCT4067?

Part Number: CD74HC4067

Hi guys,

are there protection diodes inside that CMOS devices? Which max. current are they capable if there are some? 

The question is if I need external protection diodes due to over voltage above 5.5V.

Thanks,

Markus