Other Parts Discussed in Thread: SN74LVC2G17
We have encountered a couple of instances where we suspect the A port internal protection circuitry degrades over time when connected to an open-drain signal pulled up to 5V through a 5 k-ohm resistor.
We are using the CB3T3125 as a 5V to 3.3V translator.
- Vcc = 3.3V.
- All 4 OE inputs are tied low (to GND).
- Since we only using 2 of the 4 portions (ports 1 and 2), ports 3A and 4A are also tied low; Ports 3B and 4B are floating.
After a period of extended "on time," ports 1A and 2A develop a resistance to ground. In failure scenarios, the pull-down resistance is 1.0 to 1.5 k-ohm, which, when combined with 5 k-ohm pullup, causes the signal level to not rise above 0.9 to 1.1 V. This is interpreted as a persistent logic-low signal. A "healthy" device has a measured pull-down resistance of approx. 335 k-ohm. We have also measured 15 k-ohm to GND on a part, yielding a signal level of 3.7 V. This doesn't cause a level detection failure, but indicates that the device has been degraded.
Any guidance on possible causes or mitigation techniques would be appreciated.