This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3257: 105C version

Part Number: SN74CBTLV3257
Other Parts Discussed in Thread: SN74CBTLV3253, , TMUX1309, TS3A5017-Q1, TMUX1574

Hi,

my customer is using SN74CBTLV3257 and SN74CBTLV3253, but now they need extend the operating temperature to 105C.

What's the best pin to pin upgrade part?

  • SN74CBTLV3257-EP; there is no 105 °C device for the 3253,

  • Howard,

    The SN74CBTLV3257-EP has a temperature range of -55 to 125 and is p2p with the non-EP version.

    What package are they using for the 3253? The only p2p is the TS3A5017-Q1 but it's the VQFN package only. This would be a good choice for the 3253 if powered-off protection is important. A good replacement for a non-P2P device would be the TMUX1309 if powered-off protection isn't an important feature for the customer. 

    Let me know if these work or if there's any other support you may need.
    Thanks,
    Rami 

  • Hi Howard,

    TMUX1574 is a newer device and a replacement for the SN74CBTLV3257 device. The device is available in industry standard TSSOP, uQFN and small SOT-23 leaded package. This device has wider supply voltage. higher bandwidth and supports -40C to 125C temperature.

    Additional features include 1.8V logic compatibility, Fail-safe logic (control pins can be powered before supply), and Powered-off protection.

    Thank you,


    Sandesh