This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1208: Risk of overvoltage on D/Sx pins due to high VDD

Part Number: TMUX1208

Hello,

I intend to use TMUX1208PWR to interface to and ADC with low supple voltage (1.8V)

TMUX1208's VDD=5V.

Is there a scenario (eg. power sequence) at which the 5V rail may leak to D/Sx pins and cause overvoltage on ADC?

Thanks,
David.