Other Parts Discussed in Thread: TPD2E2U06, TVS0500
Hi all,
I see that the device has internal diode clamps for protection. But what is the purpose of diode clamp , is it for continuous over voltage or transients like surge or EFT. If we suppose diode clamps are for continuous overvoltage protection on the pin, then what is the surge or EFT capacity of the pins. Can i use an external TVS diode with clamp level of 14V for surge protection